This product requires use of a browser that supports JavaScript 1.2, and that you run with scripting enabled.

Knowledge Base

Solution 37336: Troubleshooting a TI-73 Family, TI-80, TI-81, TI-82, TI-83, TI-85, TI-85 and TI-86 Graphing Handheld That Will Not Turn On or Function Properly.
Type   Question and Answer
Last Updated   15-DEC-2020 12:40:04

What troubleshooting steps can I try if the TI-73 Family, TI-80, TI-81, TI-82, TI-83, TI-85, TI-85 and TI-86 graphing handheld will not turn on or function properly?

Please Note: Information on battery precautions and replacement can be found in the case entitled "Instructions for Replacing Batteries In a TI Graphing Calculator".

Please ensure that there are no buttons that are stuck down below the keypad.

Additional Note: The resets described in the troubleshooting steps below may cause a loss of  applications, programs, and data. If at all possible please create a backup using TI Connect™ first.

1) Remove all AAA batteries and reinsert them according to the polarity (+ and -) diagrams. Batteries are installed upside down, then right side up, then upside-down, then right side up, which may be different from other products.
2) Press and release the [2ND] key followed by pressing and releasing [UP] arrow. Repeat a few times. Sometimes the calculator is actually ON but looks like it is not if the contrast is turned all the way down.
3) Try a fresh new set of AAA batteries, all from the same package.
4) Turn the graphing calculator on and try to adjust the display contrast if necessary, press and release the [2ND] key followed by pressing and releasing [UP] arrow. To adjust or lighten the display, use [DOWN].
5) Remove one of the AAA batteries. Press and hold [ON] for 20 seconds. Reinsert the AAA battery and then press [ON].
6) Remove all of the batteries including the round lithium battery for 5 minutes. After the 5 minute period, reinsert all of the batteries and press [ON]. Adjust the contrast if necessary (step 2).

Access the link following for detailed information regarding warranty coverage.

If the suggestions do not alleviate the problem, please contact TI-Cares for information regarding service.

Related Categories
Feedback
Is this solution useful in resolving your question or problem ?   No   Yes