This product requires use of a browser that supports JavaScript 1.2, and that you run with scripting enabled.

Knowledge Base

Home > Product Usage > > Solution 21852
Solution 21852: Calculating the Present Value of a Perpetuity (Infinite Annuity) on a TI-83 Family, TI-84 Plus Family, or TI-Nspire™ Handheld in TI-84 Plus Mode.
Type   Question and Answer
Last Updated   25-JUN-2020 15:58:35

How can I calculate the present value of a perpetuity (infinite annuity) on a TI-83 family, TI-84 Plus family, or TI-Nspire handheld in TI-84 Plus mode?

Sometimes when dealing with annuities, there are those that pay forever instead of for a specific period of time. Hence, they are called perpetuities or infinite annuities. Since these units do not have a way to specify an infinite number of periods for N, the calculation involves the fact that the present value of a cash flow far enough into the future is going to be approximately $0. This means that futuristically the cash flows no longer add anything to the present value. Therefore, selecting a large number of payments yields a close approximation to a perpetuity.

For example, the payment is $5,000 per year and the interest rate is 9% annually. Since it is a perpetuity, the user can select 500 as N. First, access the TVM solver by pressing [APPS] [ENTER] [ENTER]. On the TI-83, press [2nd] [FINANCE] [ENTER]. Input the following:

Next, place the cursor next to PV and press [ALPHA] [SOLVE] to compute the present value:

The present value is $-55,555.56.

Note: There is not a way to find the future value of a perpetuity because the cash flows never end.

Please see the TI-83 family and TI-84 Plus family guidebooks for additional information.

NOTE: TI-Nspire handheld in TI-84 Plus mode users may refer to the TI-84 Plus family guidebook.

Related Categories
Feedback
Is this solution useful in resolving your question or problem ?   No   Yes