This product requires use of a browser that supports JavaScript 1.2, and that you run with scripting enabled.

Knowledge Base

Solution 13884: Press-To-Test Functionality Available For TI-84 Plus Family and TI-Nspire™ Handheld in TI-84 Plus Mode Graphing Calculators.
Type   Question and Answer
Last Updated   02-AUG-2012 15:26:45

What is Press-To-Test and how is it activated/disabled?

All TI-84 Plus family calculators and TI-Nspire Handhelds in TI-84 Plus mode have a special key sequence that students and teachers can use to prepare a student calculator for exams where flash applications, programs and other files are not allowed. This feature is called Press-to-Test, and it is similar to the [2nd] [MEM] [RESET] key sequence for deleting all files from the calculator before an exam.

The main difference is that the Press-to-Test function temporarily disables flash applications, rather than deleting them. After the exam, applications and programs can be restored easily for classroom use.

With the TI-84 Plus turned off, press and hold down the left and right arrow key and press [ON] (all three keys must be pressed at the same time).The Reset Options screen displayed depends on the operating system the calculator has:

Version 2.53MP and earlier                       Version 2.55MP

• By default, the angle mode is set to Degree, and Stat Diagnostics are On. Version 2.55 MP has options to disable logbase and summation functionality.
• To change the default settings, move the cursor over the desired setting and press [ENTER].
• Press [ZOOM] (beneath OK on the screen) to select OK. The Reset Complete screen displays the selected options.

Version 2.53MP and earlier                       Version 2.55MP

• Press [APPS] to verify that Apps have been disabled.

Re-enabling Apps and Programs

Student's calculators disabled using the Press-to-Test method can be re-enabled by sending or receiving a list to the calculator.  However, any file sent will work to re-enable the Apps and Programs on the calculator. The quickest way to re-enable two calculators in Press-to-Test mode will be to link the two calculators and transfer a list.

Please see the Press-to-Test guidebook for additional information.

Product

  • TI-84 PLUS
  • TI-84 PLUS SILVER
  • TI-84+ SILVER VSC
Related Categories
Feedback
Is this solution useful in resolving your question or problem ?   No   Yes