This product requires use of a browser that supports JavaScript 1.2, and that you run with scripting enabled.

Knowledge Base

Solution 31211: Troubleshooting and Setting up the TI-Navigator™ Classroom Network.
Type   Question and Answer
Last Updated   16-JAN-2014 10:54:09

What steps do I take to troubleshoot and setup the TI-Navigator Classroom Network?

Since the TI-Navigator Classroom Network consists of multiple components steps to troubleshoot and setup the system are broken up into the different components that comprise the system.

Please click on the component you are having issues with from the list of articles listed below:

TI-Navigator Software:

For assistance installing or troubleshooting the TI-Navigator Software please visit Knowledgebase Article #31351.

Please Note: The steps below only correspond to Nav-AP-US Access Point pictured below. For assistance with the Type I and Type II Access Points please scroll further down in the Knowledgebase Article.

TI-Navigator Access Point:

If you require assistance setting up the TI-Navigator Access Point for the first time or at the beginning of the school year please visit Knowledgebase Article #33091

If you have previously setup your TI-Navigator Access Point but are having issues detecting the Access Point please visit Knowledgebase Article #26650

TI-Navigator Wireless Hubs:

If you require assistance setting up the Wireless Hubs for the first time please visit Knowledgebase Article #33092

If you have previously setup your Wireless Hubs but are having issues detecting some or all of your handhelds please visit Knowledgebase Article #23950

Please Note: The steps below only correspond to Type I and Type II Access Points pictured below. For assistance with the Nav-AP-US Access Point please scroll further up in the Knowledgebase Article.

  

TI-Navigator Initial Setup:

If you require assistance configuring Type I and Type II system type and operating channel please visit Knowledgebase Article #32951

TI-Navigator Network Adapter:

If you require assistance setting up the TI-Navigator Network Adapter for the first time or at the beginning of the school year please visit Knowledgebase Article #32952

If you have previously setup your TI-Navigator Network Adapter but are having issues detecting the Network Adapter please visit Knowledgebase Article #10285

TI-Navigator Access Point:

If you require assistance setting up the TI-Navigator Access Point for the first time or at the beginning of the school year please visit Knowledgebase Article #32914

If you have previously setup your TI-Navigator Access Point but are having issues detecting the Access Point please visit Knowledgebase Article #10240

TI-Navigator Wireless Hubs:

If you require assistance setting up the Wireless Hubs for the first time please visit Knowledgebase Article #33011

If you have previously setup your Wireless Hubs but are having issues detecting some or all of your handhelds please visit Knowledgebase Article #23950

If you need assistance with any of the steps listed above or if the troubleshooting does not correct your issue please call the TI-Navigator support line at 1-866-846-2844 Monday-Thursday 8:00 AM - 7:00 PM and Friday 10:00 AM - 7:00 PM Central Standard Time or fill out the TI-Cares™ Customer Assistance Form.

Related Categories
Feedback
Is this solution useful in resolving your question or problem ?   No   Yes